Controller types

Open the
Controller Properties
dialog box,
General
tab and select
Change Controller
.
Change controller types for the project from the
Controller Properties
dialog box,
General
tab. When changing controllers, the options are:
  • Change the controller type.
  • Select a software version (if more than one version of Logix 5000™ is installed on the computer).
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal