Use the software with DeviceNet modules
If you selected the DeviceNet module type when you opened or created the current configuration, you can configure a DeviceNet module (1756-DNB) using the ControlLogix Gateway configuration tool. You can create and save configuration files associated with the DeviceNet module to a disk.
Provide Feedback