View DeviceNet port diagnostics

If you select a DeviceNet module, you can view information about the module's DeviceNet port by selecting the
Port Diagnostic
tab. The
Port Diagnostic
tab provides the following counter information about your module:
Network Configuration:
Counter Name
Description
Network address
Address of the Node on the network.
Baud Rate
Current baud rate for the selected device.
Diagnostic Counters:
Counter Name
Description
Bus-Off Count
Number of times the device has been off-line due to a high number of network errors.
Arbitration Loss Count
Number of times a message transmission was attempted, but not sent due to a lower priority.
Overload Count
Number of times the device has detected an overload condition on the network.
Bit Errors
Number of times the monitored bit value in a message was different than the sent bit value.
Stuff Errors
Number of times the device detected a bit stuffing error on the network.
Ack Errors
Number of times the transmitted message was not acknowledged at the link level.
Form Errors
Number of times a fixed-form bit field contains one or more illegal bits.
CRC Errors
Number of times the device calculated a different CRC value than the transmitter of the message.
Rx Messages Lost
Number of times a received message has been lost due to an overwrite by a newer message.
Warning Errors
Number of times that the error counters in the device have reached the warning level. The warning level indicates an approach to the Bus-Off condition.
Rx Error Level
Receive error counter. This counter increases when a receive error is detected, and decreases when valid packets are received.
Tx Error Level
Transmit error counter. This counter increases when a transmit error is detected, and decreases when a packet is successfully transmitted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal