Lock and unlock counter displays
To lock or unlock the diagnostic counters, you must be on a port diagnostics,
Connection Manager
, or Backplane
tab. To hold the counter display at the current value, click Lock Counters
. When you click Lock Counters
, the counters within the module continue to increase. The display updates after you select this button again. The button serves as a toggle for locking and unlocking the diagnostic counter displays. The first time you select it, the displays are locked. The second time you select it, the displays are unlocked.Provide Feedback