DeviceNet connection manager diagnostics

Field
Description
Requests
Number of open/close connection requests this module has received.
Format Rejects
Number of open/close connection requests this module has rejected because the request was not formatted correctly or because some parameter value was not within a supported range of values.
Resource Rejects
Number of open connection requests this module has rejected because the module did not have enough resources (buffers, link bandwidth, or CPU utilization) to honor the request.
Other Rejects
Number of forwarded open/close connection requests a module rejects.
Connection Timeouts
Number of connections not explicitly closed by the connection originator, but closed by this module because they were not being used.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal