Create and edit the routing table

To address 1756-DH485 or 1756-DHRIO modules, you must provide a path or route by setting up a
routing table
. The routing table translates link ID and node address information into path or routing information.
To create a routing table:
  1. Select the
    Routing Table
    tab.
  2. Add
    ,
    delete
    ,
    or edit modules as necessary.
  3. Click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal