Edit a module's information

When editing a module in the routing table, the dialog box that opens depends on the module type you have selected.
To edit the module information:
  1. In the
    1756-DHRIO interface
    , select the
    Routing Table — Configuration
    tab.
  2. Select the module (or part of the module) that you want to edit.
  3. Select
    Edit > Edit Module
    .
  4. Change the module information as appropriate:
    If you are changing information for this module type:
    Refer to:
    1756-DHRIO
    DH+ Bridge
    1756-ENET
    1756-CNB
    Backplane
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal