Delete modules from the routing table
To delete a module (and the existing modules that follow it) from the routing table:
- In theDHRIO interface, select theRouting Table — Configurationtab.
- Select the module you want to delete.TIP:You cannot delete the 1756-DHRIO module that is currently being configured.
- SelectEdit > Delete Module.
- To delete the module (and any existing modules that follow it), clickYes.
Provide Feedback