Add new modules to the routing table
If you are: | Do this: |
Adding a ControlNet module |
|
Adding an Ethernet module | |
Adding a DH+ module |
|
Adding a module to the ControlLogix backplane |
If you do not want to assign a link ID, enter
0
. DH+ bridge modules allow a list of link IDs to be entered. Link IDs are all the links that can be reached through that bridge. Each link ID in a system must be unique. Workstations can have a link ID that is used to deliver unsolicited requests to applications on that workstation, where each application has its own station address.Provide Feedback