About the ControlLogix Gateway Configuration tool
How do I access this tool?
For the modules that are supported by ControlLogix Gateway Configuration Tool, right click the module in the RSWho browser tree, and select Module Statistics in the context menu.
The modules, which are supported by ControlLogix Gateway Configuration Tool, include but not limit to: 1756-ENBT, 1756-ENET, 1756-EWEB, 1756-EN2T, 1756-EN2TSC, 1756-EN2TR,1756-EN3TR, 1768-ENBT, 1768-EWEB,1788-ENBT, 1783-ETAP, 1734-AENT, 1738-AENT, 1794-AENT, 1747-AENTR, 1734-AENTR, 1738-AENTR,1794-AENTR, SoftLogix5800, 1791ES-IB8XOBV4, 1791ES-IB16, 1732E Ethernet/IP ArmorBlock I/O, 1752-L24BBBE, Micro820, and Micro850.
The ControlLogix Gateway Configuration Tool provides the following information about the modules in your ControlLogix Gateway:
- General module information
- Status and diagnostics information
- Configuration information
In addition, the tool allows you to:
- Set or change the configuration of ControlNet, DeviceNet, Ethernet, 1756-DHRIO, or 1756-DH485 modules
- Access diagnostic information on ControlNet, DeviceNet, and Ethernet Bridge modules
- Save and restore configuration data
Provide Feedback