Use the software with ControlNet modules

If you selected the ControlNet module type when you opened or created the current configuration, you can configure a ControlNet module (1756-CNB, 1756-CNBR, 1756-CN2R) using the ControlLogix Gateway configuration tool. You can create and save configuration files associated with the ControlNet module to a disk.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal