OPCGroup object

The OPCGroup object maintains state information and provides the mechanism to give data acquisition services for the OPCItems collection that the OPCGroup object references. The following properties, methods, and events are included in the OPCGroup object:
Properties
Name
IsActive
IsSubscribed
ClientHandle
ServerHandle
UpdateRate
OPCItems
Methods
SyncRead
SyncWrite
AsyncRead
AsyncWrite
AsyncRefresh
Events
DataChange
AsyncReadComplete
AsyncWriteComplete
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal