OPCGroups collection
The OPCGroups collection is an automation collection containing all of the OPCGroup objects this client has created within the scope of the OPCServer that the Automation Application has connected to via the OPCServer.Connect() The following properties and methods are included in the OPCGroups collection:
Properties
Count
DefaultGroupIsActive
DefaultGroupUpdateRate
Methods
Item
Add
Remove
RemoveAll
Provide Feedback