OPCServer object
The OPCServer object is an instance of an OPC Server. You must create an OPCServer object before you can get references to other objects. It contains the OPCGroups collection and creates OPCBrowser object. The following properties and methods are included in the OPCServer object:
Properties
ServerName
OPCGroups
VendorInfo
ServerNode
Methods
Connect
Disconnect
GetErrorString
GetOPCServers
CreateBrowser
Provide Feedback