OPC Custom Interfaces
As an OPC Data Access 2.05 server, RSLinx Classic provides all the required interfaces as defined in the OPC Foundation's Data Access 2.05 Specification. The defined interfaces are as follows:
OPCServer Object
OPCGroup Object
Provide Feedback