OPCBrowser object

The OPCBrowser object browses item names in the server's configuration. There exists only one instance of an OPCBrowser object per instance of an OPC Server object. The following properties and methods are included in the OPCBrowser object:
Properties
Organization
Filter
DataType
CurrentPosition
Count
AccessRights
Methods
Item
ShowBranches
ShowLeafs
MoveToRoot
MoveUp
MoveDown
GetItemID
GetAccessPaths
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal