OPCItems collection

The OPCItems collection is an automation collection that contains all of the OPCItem objects this client has created within the scope of the OPCServer, and corresponding OPCGroup object that the Automation Application has created. The following properties and methods are included in the OPCItems collection:
Properties
DefaultRequestedDataType
DefaultAccessPath
Count
Methods
Item
AddItems
Remove
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal