OPCItem object

The OPCItem object is an automation object that maintains the item's definition, current value, status information, and last update time. Note that the Custom Interface does not provide a separate Item Object. The following properties and methods are included in the OPCItem object:
Properties
Value
Quality
ClientHandle
ServerHandle
AccessPath
ItemID
IsActive
RequestedDataType
TimeStamp
Methods
Read
Write
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal