- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Screen style
Style for screens
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Background color | BackgroundColor | If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property | |
Border color | BorderColor | Color of the polygon border | |
Border thickness | BorderThickness | Border thickness in pixels |
Provide Feedback