FactoryTalk Optix Studio CLI

FactoryTalk Optix Studio CLI

Use the command-line interface (CLI) of
FactoryTalk Optix Studio
to perform actions without having to interact with the graphical user interface (GUI).
TIP: Running CLI commands is useful for scripting and automating pipelines.
To run a command, see Run a CLI command. To learn about the available commands, see CLI commands.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal