Set up Smart Objects

Set up Smart Objects

  1. Create a FactoryTalk Optix project.
  2. Go to and in the
    Scripts
    folder select the
    Smart Objects
    library.
  3. In Project view, drag the library to the
    NetLogic
    folder.
    Your NetLogic foler should be updated with the following objects:
    -SmartObjects[Folder] -Types[Folder] -SmartObjectImporter[DataType] -SmartObjectsDesignTime[NetLogic Script] -SmartObjectRuntime[NetLogic Script] -Status[Variable]
  4. From The Product Compatibility and Download Center (PCDC) download package
    Sync_Objects_
    vX.YY.ZZ
    .zip
    .
    where
    vX.YY.ZZ
    is the current version of the file, for example
    v1.23.45
  5. Save and extract the package on a local drive.
  6. Open
    config.xml
    , and modify required settings:
    1. Enter the FactoyTalk Optix Studio location path.
    2. Enter the FactoryTalk Optix project location path.
  7. Run the script file
    install.bat
    .
    Local NuGet pacakge is installed on your FactoryTalk Optix project defined in the
    config.xml
    in 6. The script also downloads and installs to the project two external NuGet packages:
    NetMQ 4.0.1.13
    and
    Newtonsoft.Json 13.0.3
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal