Use OPC Test Client to test Remote FactoryTalk Linx Gateway

OPC
Test Client verifies that Remote
FactoryTalk Linx Gateway
is able to establish a data connection to a remote
OPC
DA server. This utility is installed as part of Remote
FactoryTalk Linx Gateway
installation on the
FactoryTalk Linx Gateway
product DVD.
Prerequisites:
  • Install Remote
    FactoryTalk Linx Gateway
    on the computer that hosts the
    OPC
    DA client.
To use OPC Test Client:
  1. Ensure the remote
    OPC
    DA service is running.
  2. Start
    OPC
    Test Client by selecting
    Start > All Programs > Rockwell Software > RSLinx > Tools >
    OPC
    Test Client.
  3. From the
    OPC
    Test Client menu, select
    Server > Connect
    .
  4. Select an
    OPC
    DA server from the
    Located Servers
    list or select
    Browse
    to find an
    OPC
    DA server, then select
    OK
    .
  5. Select
    Group > Add Group
    to add a group, which is a collection of tags with the same update (scan) rate. Name the group and specify an update rate, then select
    OK
    .
    TIP:
    The server will return the group update rate closest to the rate requested by the client. The supported update rates are: 10, 20, 50, 100, 250, 500, 600, 700, 800, 900, 1000, 2000, 3000, 4000... to 60000 ms.
  6. Click
    Item > Add Item
    to open the Browse window to enable browsing for tags.
  7. Locate and expand the root node.
  8. Click the controller containing the tags you want to browse.
  9. Click the Online folder to expose the controller tags.
  10. Select the tags you want to access (up to, but not exceeding, the activation count).
  11. Click
    OK
    to add the tags and start collecting data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal