Tools for troubleshooting FactoryTalk Linx Gateway
To isolate, diagnose, and correct any problems using
FactoryTalk Linx Gateway
, use the following troubleshooting tools:Tool | Description |
|---|---|
FactoryTalk Linx Gateway Configuration | The Global Settings in the FactoryTalk Linx Gateway Configuration |
FactoryTalk Diagnostics | FactoryTalk Diagnostics provides the ability to log errors, warnings, and other status messages generated throughout a FactoryTalk -enabled system to a central location called an event log.If you encounter a problem, you can review the events in the log that led up to the problem to assist in determining the cause. Or you can monitor the log to identify potential problems and take corrective action before a problem occurs. Note that FactoryTalk Diagnostics messages show for the local workstation only.FactoryTalk Audit records changes to FactoryTalk Directory resources made by users during the design, management, or operation. Logs to multiple output formats for change management and regulatory compliance. |
FactoryTalk Diagnostics Counter Monitor | FactoryTalk Diagnostics Counter Monitor provides the ability to check the status of tags, and to monitor the runtime values of counters and strings that are made available by network clients for diagnostic purposes. The FactoryTalk Diagnostics event log and Help are integrated into this tool. This utility is installed automatically with FactoryTalk Services Platform . |
FactoryTalk Live Data Test Client | FactoryTalk Live Data Test Client allows you to:
This tool is installed automatically with FactoryTalk Services Platform . |
MQTT broker | Testing confirmed FactoryTalk Linx Gateway's MQTT interface can deliver data to the listed brokers. Each application should perform testing to confirm the selected broker can achive the desired application capacity and performance requirements. |
MQTT client | Testing confirmed FactoryTalk Linx Gateway's MQTT interface can deliver data to the listed clients via a broker. These clients are helpful to manually evaluate the configuration. Each application should perform testing to confirm the selected client, and broker can achieve the desired application capacity and performance requirements. |
Third party OPC UA sample clients |
Provide Feedback