Use FactoryTalk Live Data Test Client to test an OPC DA server connection

FactoryTalk Live Data
Test Client is a utility that enables you to test your
OPC
DA connection after you have configured
FactoryTalk Linx Gateway
. This utility is installed automatically with
FactoryTalk Services Platform
. This tool allows you to connect to
OPC
DA servers directly, or view
OPC
DA data received and processed through
FactoryTalk Live Data
.
Refer to the
FactoryTalk Live Data Test Client
Help for information on how to use the
FactoryTalk Live Data
Test Client.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal