Custom UA Namespace

How do I open Custom UA Namespace?
  1. From the
    Start
    menu, select
    Rockwell Software
    >
    FactoryTalk Linx Gateway Configuration
    .
  2. On
    OPC UA Server
    , select
    Custom namespace
    .
  3. On the left pane, select
    Custom Namespace
    .
Use the
Custom Namespace
editor to create tag definitions for the OPC UA interfaces and bind or map them to system data points to provide consistent names for different components or to organize the data to comply with an industry standard, for example, OPC UA Companion Specifications.
If you do not use
Tag Browser
to add or edit a tag in the
Custom Namespace
editor, you must ensure that the tag’s data type is the same as the data source, such as the Logix controller, or OPC UA server connected via the FactoryTalk Linx OPC UA Connector.
If you change a tag’s data type in a controller, you must ensure that the tag’s data type in the
Custom Namespace
editor is the same as that in the controller. Otherwise, an error message "BadTypeMisMatch" appears in the UA clients when a tag is requested, or a FactoryTalk Diagnostic message will be generated listing the type mismatch for a write operation.
TIP:
The UA tag list does not support FactoryTalk Diagnostic Audit message.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal