Naming conventions in Custom UA Namespace

The following table shows the naming conventions in the
Custom UA Namespace
.
Type
Limitation
Maximum length
Case-sensitive (Yes or No)
Namespace name
The name must consist of any character from the following:
  • 0 - 9
  • a - z
  • A - Z
  • _
256
Yes
Tag name*
The name must consist of any character from the following:
  • 0 - 9
  • a - z
  • A - Z
  • _
  • @
256
No
Tag descriptions
The descriptions cannot contain quotation marks.
256
N/A
Folder name*
The name must consist of any character from the following:
  • 0 - 9
  • a - z
  • A - Z
  • _
256
No
Type name*
The name must consist of any character from the following:
  • 0 - 9
  • a - z
  • A - Z
  • _
256
Yes
Type descriptions
The descriptions cannot contain quotation marks.
256
N/A
Type member name*
The name must consist of any character from the following:
  • 0 - 9
  • a - z
  • A - Z
  • _
256
Yes
Type members description
The descriptions cannot contain quotation marks.
256
N/A
*Upper and lower case letters in names are helpful for presentation only. Names are not case-sensitive.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal