Certificate Management
How do I open Certificate Management?
- From theStartmenu, selectRockwell Software>.FactoryTalk Linx GatewayConfiguration
- UnderOPC UA Sever, selectCertificate Management, and then selectIncoming CertificateorOutgoing Certificate.
Use
Certificate Management
to view FactoryTalk Linx Gateway
OPC
UA server certificate information.FactoryTalk Linx Gateway
creates a default, self-signed security certificate during installation. The security certificate is stored at C:\ProgramData\Rockwell\FactoryTalk Linx Gateway\PKI\own\cert_ftgw_opcua_server.der
on the host computer for the FactoryTalk Linx Gateway
server. A custom security certificate can be created by generating a certificate signing request (CSR) in FactoryTalk Linx Gateway
and signed by an external trusted security authority and then imported to FactoryTalk Linx Gateway
to replace the default certificate.Incoming Certificate
Button | Description |
|---|---|
Refresh | Refreshes to display the latest certificates. |
Manage Access | Limits access to security certificate management operations to administrators or individuals approved by an administrator. This function is only available to Administrator. To add user or group:
|
Import | Specifies and import the certificate to be used as incoming certificate or outgoing certificate. |
Reject | Moves the specific certificates from Trusted Certificates list to Rejected Certificates list. The client(s) cannot communicate with FactoryTalk Linx Gateway . |
Remove | Removes the specific certificates from Trusted Certificates list or Rejected Certificates list. The clients cannot communicate with FactoryTalk Linx Gateway . |
Trust | The specific certificate is added to Trusted Certificates list and the client can communicate with FactoryTalk Linx Gateway . |
Outgoing Certificate
Button | Description |
|---|---|
Refresh | Refreshes to display the latest certificates. It is only available when
enabling the certificate management by FactoryTalk Policy Manager . |
Manage Access | Limits access to security certificate management operations to administrators or individuals approved by an administrator. This function is only available to Administrator. To add user or group:
|
Create CSR | Creates a Certificate Signing Request (CSR) and save the request as a CSR file. |
Import | Specifies and import the certificate to be used as incoming certificate or outgoing certificate. |
Regenerate | Creates another certificate to renew the valid period. |
Certificate properties
Field | Description |
|---|---|
Name | Displays the name of the security certificate. |
Location | Displays the path to the security certificate on the FactoryTalk Linx Gateway computer. |
Application Name | Displays the application from where the certificate is presented. |
Organization | Displays the organization name that submitted to CA when requesting the certificate. |
Application URI | Displays the FactoryTalk Linx Gateway application URI associated with the security certificate. |
Domain | Displays the domain name. |
Subject Name | Displays the subject properties on the certificate. For example, Common Name (CN). |
Valid From | The date and time when the security certificate is valid. |
Expiration Time | The date and time when the security certificate expires. |
Thumbprint | A short sequence of bytes created by applying the cryptographic hash function to identify a certificate. |
Provide Feedback