Import a certificate
When establishing a connection between an OPC UA client and
FactoryTalk Linx Gateway
, the certificates from both sides need to be presented and trusted separately.The user can select to manually import an incoming certificate and a custom outgoing certificate (Prior to version 6.20.00, an outgoing certificate is created by
FactoryTalk Linx Gateway
by default).Prerequisites
- TheFactoryTalk Linx Gatewayserver and the OPC client must be installed on the same workstation.
To import a certificate
- FromFactoryTalk Linx GatewayConfiguration, underCertificate Management, selectIncoming CertificateorOutgoing Certificate, and then selectImport.
- After the file selection dialog box opens, select the certificate file, and then clickOK.TIP:When importing certificates, select the following supported file formats:
- .pem
- .cer
- .crt
- .der
- .p7b
- .p7c
- .p12
- .pfx
- (Optional) If an outgoing certificate requires a password to decrypt, enter the correct password to continue.TIP:You can useManage Accessto limit access to security certificate management operations to administrators or individuals. This function is only available to Administrator. For more details, see Certificate Management.
Provide Feedback