Read multiple array items from the OPC UA server

FactoryTalk Linx Gateway
supports multiple ways to access OPC UA array data.
FactoryTalk Linx Gateway
provides an advanced option to enumerate all elements of array data. When this option is enabled, the client will see namespace entries for all of the items in arrays. The client can then access these items individually, while indexed access of multiple elements is not supported from the enumerated items.
When
Tag list and structures/array access
or
Custom namespace
is turned on, you can read the following array items:
When
Folders with scalar data
is turned on, you can read the following array items:
  • Single scalar element
  • Multiple elements from a scalar array using index
    TIP: The index range should be in the format of "Starting element number, a colon and the ending element number". For example, "3:8". Multi-dimensional arrays are not currently supported using the index capability.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal