Historian WebTrend

Historian WebTrend is a web server-based application that allows you to visualize, access, monitor, and analyze data from Asset Framework or Data Archive using modern web browsers.
Currently, Historian WebTrend only supports
FactoryTalk® Historian Site Edition
as the data source.
Supported browsers
  • Microsoft®
    Edge™
  • Google®
    Chrome™ browser
  • Apple® Safari®
Supported display resolutions
  • If running this software with a 2K or 4K high-resolution display with scaling up to 125%, you can expect acceptable results. For optimal user experience, use the Windows recommended scaling rate for 2K, 4K, or 8K displays.
  • If running this software at the minimum resolution, for optimal user experience, use a resolution of 1024 x 768.
Rockwell Automation®
recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal