Export and reuse trends from FactoryTalk VantagePoint
Use the WebTrend Migration Tool to migrate trends from
FactoryTalk® VantagePoint®
to
Historian WebTrend. For more information, see WebTrend Migration Tool documentation in
FactoryTalk Historian SE version 12.01.00 installation
package\Redist\OtherComponents\WebTrendMigrationTool1.0.0.zip\Docs
.Provide Feedback