Back up and restore the database
Back up and restore the Historian WebTrend database to ensure data availability and
continuity. Only users assigned the Administrator role can perform backups and
restorations. To preserve trends saved in
FactoryTalk Historian SE
version 12.00.00
or earlier, upgrade FactoryTalk Historian SE
to version 12.01.00, and then back up
and restore saved trends.For any problems encountered during the backup and restoration, see the log files in the
following default locations:
- C:\ProgramData\Rockwell Software\FactoryTalk Historian\Historian WebTrend Data Provider\Logs
- C:\ProgramData\Rockwell Software\FactoryTalk Historian\Historian WebTrend\Logs
Provide Feedback