Sign in to Historian WebTrend
Sign in to access and use all the features of Historian WebTrend.
When first signing in to Historian WebTrend, you may meet two kinds of notifications. See
the following table to view the cause and resolution.
Message | Cause | Resolution |
|---|---|---|
Authentication failed. Wait n seconds and try
again. |
|
|
|
| |
Authorization failed. Wait n seconds and try again. |
|
|
To sign in to Historian WebTrend
- Open a browser, and enter either of the following URLs:
- https://<hostname>:7080/webtrendThe<hostname>is the name of the computer with the Historian WebTrend server installed.
- https://<IPv4 Address>:7080/webtrend
- On the authentication page, enter the Windows-linked FactoryTalk username and password.
- SelectLogin.Historian WebTrend authenticates throughFactoryTalk Directoryby retrieving the port number fromC:\ProgramData\Rockwell\FTWeb\ft-web-config.json. If this JSON file is removed or the port number changes, restart the computer. If Historian WebTrend andFactoryTalk Directoryare installed on separate computers, you must restart both computers.
Provide Feedback