Introduction to the Material Server

For ease of understanding, and for tutorial purposes, this guide refers to configuring and using the sample files that are installed with
FactoryTalk Batch
. The SampleDemo folders contain complete area models and recipes for a simulated plant. Before running the demonstrations:
  • Configure the Network Editor to recognize the material database
  • Add a
    FactoryTalk
    Security user
  • Configure the
    FactoryTalk Batch
    Server to recognize the required project directories
  • Select the initialization path and file name
  • Start the
    FactoryTalk Batch
    Server and the
    FactoryTalk Batch
    Phase Simulator
    TIP:
    This guide outlines the configuration and use of the SampleDemo2 demonstration files. Because these files are used as an example throughout the guide, it is recommended that you follow the directions for using this demonstration step by step.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal