Set up the sample demonstrations

The installation process placed the
SampleDemo1
and
SampleDemo2
folders in the
BATCHCTL
share on your hard drive. Within each of these
SampleDemo
folders are four subfolders that contain the files for the area model. To run the sample demonstrations, configure the Network Editor to locate the material database, add a
FactoryTalk
Security user, configure the
FactoryTalk Batch
Server to locate the area model, and then verify the recipes in the area model.
IMPORTANT:
The default databases MaterialBasedRecipe and SAMPLE2_Materials cannot be removed from SQL Server. You are free to add another database and use it for production or test, but you must keep the originally installed databases intact even though they are not being used.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal