Configure the Network Editor
Configure the Material Server with the location of the SQL database that contains the materials for the SampleDemo2 recipes.
- SelectStart> Rockwell Software >, and then selectMaterial ManagerNetwork Editor. The Network Editor window opens.
- Select the Material Server.IMPORTANT:Administrator privileges are required to perform this procedure.
- SelectConfigure. TheConfigure MaterialTrackdialog box opens.
- In theMaterialTrackDatabasebox, typeSAMPLE2_MATERIALS, and then selectOK.
- SelectSynchronize.
- SelectFile>Exit, and then clickYesto exit the Network Editor.
Provide Feedback