Start the
FactoryTalk Batch
and
Material Manager
Servers

The
FactoryTalk Batch
and
Material Manager
Servers may start automatically when the computer starts. By default, the
FactoryTalk Batch
Server starts in production mode. If
FactoryTalk Batch
has not been activated, the tutorial can run in demo mode. While in demo mode, the
FactoryTalk Batch
Server runs for a two-hour period and then stops.
TIP:
The
FactoryTalk Batch
Server does not start in production mode without activation. The
Material Manager
Server starts automatically when the
FactoryTalk Batch
Server starts. See
Activating
Material Manager
for more information.
  1. To start or restart the
    FactoryTalk Batch
    Server:
    1. Select
      Start
      > Rockwell Software >
      Batch
      Service Manager
      .
      IMPORTANT:
      If you are logged in with an account that does not have administrator privileges, right-click
      Batch Service Manager
      and select
      More > Run as administrator
      to run under elevated privileges.
    2. In the
      FactoryTalk Batch
      Service Manager
      , select the
      FactoryTalk Batch
      Server if it is not listed in the
      Service
      box.
    If the
    FactoryTalk Batch
    Server is running, select
    Stop
    .
    FTB_GRG_batch_service_manager_stopped
  2. If the name of the computer where the
    FactoryTalk Batch
    Server is installed does not display in the
    Computer
    box, select the
    Select Computer
    button.
  3. In the
    Select Computer
    dialog box under
    Enter the object name to select
    , type the name of the computer where the Batch Server is installed (or select
    Advanced
    to search for a computer). Select
    OK
    .
    TIP:
    The
    FactoryTalk Batch
    Service Manager must communicate with the Windows Service Manager of the selected computer to determine what services are available. There may be a noticeable delay when establishing communications. If the Service Manager cannot communicate with the Windows Service Manager of the selected computer, a message displays.
  4. From the
    Service
    list, select
    FactoryTalk Batch
    Server
    .
    TIP:
    If
    No Batch Services
    displays in the list, the
    FactoryTalk Batch
    Server is not installed on the selected computer. See the
    FactoryTalk Batch
    Components Installation and Upgrade Guide
    for installation instructions.
  5. To start the
    FactoryTalk Batch
    Server in Demo mode, select
    Allow Demo Mode
    .
  6. Select the method to use for booting the server.
    Cold Boot
    Restarts the
    FactoryTalk Batch
    Server in a cold state. All journal data or recipe content is erased upon startup.
    Warm Boot
    Restarts the
    FactoryTalk Batch
    Server, restoring the set of batches that were on the batch list when the server previously terminated.
    Warm All Boot
    Restarts the
    FactoryTalk Batch
    Server only if it is able to restore all of the batches to the batch list.
  7. Select the
    Start/Continue
    button. The Service State area changes from STOPPED to START PENDING. After a few moments, RUNNING displays and the light changes to green. The Material Server starts automatically with the
    FactoryTalk Batch
    Server.
    The
    FactoryTalk Batch
    Phase Simulator starts automatically. Minimize the window.
  8. Select
    Close
    to close the
    FactoryTalk Batch
    Service Manager.
    TIP:
    If conversation becomes LOST while running in Demo mode, make sure that the Simulator is running and try starting the server(s) again. See
    Starting the
    FactoryTalk Batch
    Phase Simulator
    for more information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal