Unassigned
The
Unassigned
tab lists the devices that have not been assigned the IP address. Use the Unassigned
tab to configure IP address or set up rules for automatic IP assignment.Unassigned tab actions
Button | Descriptions |
|---|---|
Add to Configuration | Used to add a MAC/IP address for the selected item to the configuration list. |
Commission from range | Used to automatically assign IP addresses from a contiguous user defined set. |
Commission from list | Used to guide the device startup sequence and IP address assignment process from items in the configuration list that do not have MAC address assigned. |
Delete | Used to remove a device from the Unassigned list. |
Export | Used to save the unassigned device list in a CSV file. |
Filter | Used to limit the view of the Unassigned list to a set matching user entered text. Case-insensitive. |
Expand | Used to adjust the window to only view the device list. |
Block MAC | Used to add a MAC address to the Blocked MAC list. Any future BOOTP/DHCP requests from that address will not be listed in the Unassigned list and will not be assigned an IP address.Tip : Enable the MAC address blocking function in Settings . |
View Assigned | Used to open and view the assigned list on the Unassigned tab. |
Device properties
Field | Descriptions |
|---|---|
Host name | The device name. |
IP | The IP address for this device. If blank, the device is not able to communicate on the network. |
MAC | The MAC address for this device. Assigned to the device when manufactured and provided from the device when a BOOTP/DHCP request is made. |
Request type | The protocol that the device uses to request IP address (BOOTP/DHCP). |
Status | The IP address assignment status and the reason for failed assignments will be listed. The possible statuses include:
|
Request date | The latest time that the device requested the IP address from the BOOTP/DHCP server. |
Request count | The total number of times that the device requested the IP address from the BOOTP/DHCP server. |
TIP:
- You can select any column heading to sort the list by that column.
- If text in the interface is truncated, you can hover your pointer over the item to see the information displayed as a tooltip.
Provide Feedback