Active Anonymous Connections
Description
This counter indicates the number of anonymous OPC UA clients connected to the OPC UA server.
TIP:
The sum of Active Anonymous Connections and Available Anonymous Connections should be the value of Maximum Anonymous Connections Setting.
Location
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
- Type: 64-bit signed integer
- Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
- Updates: This value increases when an anonymous OPC UA client connects to the server and decreases when an anonymous client disconnects from the server.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback