Create a snapshot file using a command

You can create a snapshot file using a command. This provides the diagnostic counter values for the specified workstation only.
To create a snapshot file using a command:
  • In the
    Command Prompt
    window, type:
    FTCounterMonitor.exe /snapshot /wks:[target] [xmlfilename]
    For example,
    FTCounterMonitor.exe /snapshot /wks:10.88.101.2 snapshot.xml
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal