Manage target devices
    Add, remove, duplicate, and select target target devices available in the network.
The default target target device, the 
    
    
    
    
Emulator
, runs locally on the development computer. The Emulator
 is useful for testing FactoryTalk Optix Applications
 and does not require you to install the FactoryTalk Optix Application Update Service
 software.
      
     TIP: 
    The 
Emulator
 runtime stops automatically after two hours even if a valid license is present on the device. If you need to test your application for a longer period of time, export the application. See Export a FactoryTalk Optix Application.
     TIP: 
    Rebooting the 
Emulator
 is not supported so that you do not accidentally reboot a device on which Windows®
 is installed. Provide Feedback