Select a target device
    Select an already configured target device to deploy 
FactoryTalk Optix Applications
 over the network to the target device.- From the main toolbar, next to, select the target dropdown menu.Run
- (optional) InTarget device settings, to display only the active remote target devices, toggleActive remote devices.TIP: Refresh remote target devices by selectingRefresh.
- Select a target device.
- ChooseSelect.
Provide Feedback