Deploying projects
    Compile projects to 
FactoryTalk Optix Applications
 and then deploy the applications to target devices.To determine which presentation engine is required for the mode in which 
FactoryTalk Optix
 will be running, see FactoryTalk Optix runtime modes.You can manage the target devices to which you deploy 
FactoryTalk Optix Applications
. See Manage target devices and Deploy a FactoryTalk Optix Application.For target devices not accessible in the network, you can export 
FactoryTalk Optix Applications
 from FactoryTalk Optix Studio
 and then import them to target devices. See Export a FactoryTalk Optix Application and Import a FactoryTalk Optix Application.Provide Feedback