Import a FactoryTalk Optix Application
    To deploy an exported 
FactoryTalk Optix Application
, move the file to the target device and run the file.Prerequisites
- To import aFactoryTalk Optix Application
- Move the exported files to the target device.For example, attach the USB drive with the exported application to the target device.
- RunFactoryTalk Optix Applicationon the target system:- OnWindows®target devices, in thefolder, double-clickFTOptixApplicationFTOptixRuntime.exe.
- On Linux target devices, in the terminal:- Entercdto navigate to theFTOptixApplicationdirectory.FTOptixApplication
- Entersudo chmod +x FTOptixRuntimeto make the runtime executable.
- Entersudo chmod +x opensslto make the openssl library executable.
- Enter./FTOptixRuntimeto run the application.
 
- OnOptixPanel, access the web interface and then selectImportunderLoad application from USB.
 
import
    
Provide Feedback