Duplicate a target device
    Duplicate a target device to configure another similar target device. 
- From the main toolbar, next to, select the target dropdown menu.Run
- (optional) InTarget device settings, to display only the active remote target devices, toggleActive remote devices.TIP: Refresh remote target devices by selectingRefresh.
- Select a target device.
- Select.Duplicate
Configure the duplicated target device properties.
duplicate
    
Provide Feedback