Version history
    Use 
Version history
 to view all of the changes in the project
      that are committed to a repository.Version history interface

| Item | Name | Description | 
|---|---|---|
|  | User initial | The first letter of the user that committed the change to the repository. | 
|  | Commit message and details | The commit with the description of the change, the date and time of the commit.
              Select   to select the commit
              and view the changes in the commit. | 
|  | Local or remote repository indicator | Icon indicates which repository contains the commit.    Local history   Remote history | 
|  | Change details | Indicates a change in the commit from the previous version. Expand the object to
              see the highlighted values that changed in the object. | 
|  | Filter | Select either  Allto display the entire contents of the
              project, or Updatesto displays only changes to the selected
              commits. | 
version history
view history
    
Provide Feedback