Compare committed changes
    Compare two different versions of a project by selecting two different committed
      changes in 
View history
.- From the toolbar, select. View history View history
- InVersion history, two different commits to compare.TIP: The differences between the commits are highlighted.
- (optional) To toggle the content that appears inVersion history, select either:- All. Toggle to show all content in the project.
- Updates. Toggle to show only the differences between the selected commits. This is the default.
 
history
compare
    
Provide Feedback