View committed changes
    View the committed changes of the open project by viewing the project history.
- In the toolbar, select. View history View history
- InVersion history, select a commit.TIP:represents a change that is committed to the local repository and Local historyrepresents a change that is pushed to the remote repository. Local historyrepresents a change that is pushed to the remote repository. Remote historyThe changes in the commit appear highlighted. Remote historyThe changes in the commit appear highlighted.
- Expand a highlighted object to view the changes in the object.TIP: Values that change in an object are crossed out and an arrow points to the new value.
Provide Feedback