Restore a project to a commit
    Restore a previous version of a project.
     TIP: 
    When you restore a commit, the project in the local
      repository updates to include the contents of the selected commit. Restoring a commit
      permanently deletes any commits that occurred after the restored commit.
- From the toolbar, select. View history View history
- Select a commit to restore the project to.
- SelectRestore.
Version history
 closes and the open project includes the changes of the selected commit.restore project
    
Provide Feedback