Audit logs and diagnostic messages
Symptoms of problems related to audit logs and diagnostic messages:
- Audit information is not appearing in log files
- Audit messages are not being logged
- Local log stops logging new messages
- The ODBC destination does not support the required user name
- The ODBC destination stops logging new messages to a remote SQL Server
- Message chains from an ODBC Log are not reassembled for display
- Some fields are not being logged to the ODBC database
- The message logging interval for the ODBC database is ignored
- The Data Source Name is not found for the ODBC database
Provide Feedback